Real Time

PUCCH Common (Basic LTE FDD Uplink)

Additional Uplink parameters are described in Cell Parameters (Basic LTE FDD Uplink), PUSCH Common (Basic LTE FDD Uplink ), and Sounding Reference (Basic LTE FDD Uplink).

3. PUCCH Common

Set PUCCH Auto-calculate per-slot params

PUCCH Auto-calculate per-slot params

N_RB(2)

N_CS(1)

nPUCCH(1)

nPUCCH(2)

Delta Shift PUCCH

Set PUCCH Auto-calculate per-slot params

Click this cell and then the button to open the Configure PUCCH Auto-calculate window where you can set PUCCH Common parameters, including Cyclic Prefix.

PUCCH Auto-calculate per-slot params

Displays the state for automatic calculation of per-slot parameters. To change the displayed state, refer to Set PUCCH Auto-calculate per slot params above.

N_RB(2)

Displays one of the values used for generating and mapping PUCCH and DMRS PUCCH (see 3GPP TS36.211). To change the displayed value, refer to Set PUCCH Auto-calculate per slot params above.

N_CS(1)

Displays one of the values used for generating and mapping PUCCH and DMRS PUCCH (see 3GPP TS 36.211). To change the displayed value, refer to Set PUCCH Auto-calculate per slot params above.

nPUCCH(1)

Displays one of the values used for generating and mapping PUCCH and DMRS PUCCH (see 3GPP TS36.211). To change the displayed value, refer to Set PUCCH Auto-calculate per slot params above.

nPUCCH(2)

Displays one of the values used for generating and mapping PUCCH and DMRS PUCCH (see 3GPP TS36.211). To change the displayed value, refer to Set PUCCH Auto-calculate per slot params above.

Delta Shift PUCCH

Displays one of the values used for generating and mapping PUCCH and DMRS PUCCH (see 3GPP TS36.211). To change the displayed value, refer to Set PUCCH Auto-calculate per slot params above.